What is an Integrated Circuit (ICs) and Why Integrated Circuit is shortage?

Published: 23 September 2021 | Last Updated: 23 September 20216719
An Integrated Circuit(IC), or we can call it IC, chip, or microchip is a small semiconductor-based electronic device minuscule chip consisting of fabricated transistors, resistors, and capacitors, and other metallic connections required for a complete electrical circuit. In this article, we will discuss it in five aspects.
This video will tell you what is Integrated Circuit from three aspects.

What Is An Integrated Circuit (IC)

Topics covered in this article:

Ⅰ. What is an Integrated Circuit?
Ⅱ. Why Integrated Circuit is important?
Ⅲ. Integrated Circuit VS Discrete Circuit
Ⅳ. Why Integrated Circuit is shortage?
Ⅴ. Where can I find Integrated Circuit?


Ⅰ. What is an Integrated Circuit?

chip.png

Integrated circuit structure diagram

An Integrated Circuit (IC), also known as an IC chip or a microchip, is a compact semiconductor-based electronic device made up of manufactured transistors, resistors, capacitors, and other metallic connections that make up a full electrical circuit. Texas Instruments' Jack Kilby and Fairchild Semiconductor's Robert Noyce built the first integrated circuit in the 1950s. Digital, analog, and mixed integrated circuits are the three types of integrated circuits. The most common electronic gadgets and equipment use integrated circuits as their building blocks. It can be utilized in practically any electrical device or appliance on the market today. It can be found in practically every piece of modern electric equipment or appliance. This includes computers, televisions, cellphones, and even toys designed for children. ICs have transformed the world of electronics by being employed in practically every electronic equipment.

The entire circuit is built around this chip. It is about the size of a human fingernail and is quite small in compared to basic circuit circuits built of many components. Monolithic chips are currently the most widely utilized integrated circuits.



Ⅱ. Why Integrated Circuit is important?

The integrated circuit (IC) is a single unit made up of millions of electronic components such as transistors, resistors, and capacitors. Its introduction transformed the electronics industry and opened the way for gadgets such as cell phones, laptops, CD players, televisions, and a variety of other household appliances. Because of their tiny size, great reliability, and efficiency, ICs are used in practically every electronic product today. Electronic devices would be more slower and larger without ICs.

Furthermore, the widespread use of chips aided in the dissemination of advanced electronic gadgets to all corners of the globe.



Ⅲ. Integrated Circuit VS Discrete Circuit

QQ截图20210923154004.png

Differences between Discrete Circuit and Integrated Circuit

(1)The Integrated Circuit (IC) is a single unit made up of millions of electronic components such as transistors, resistors, and capacitors. Its introduction transformed the electronics industry and opened the way for gadgets such as cell phones, laptops, CD players, televisions, and a variety of other household appliances. Because of their tiny size, great reliability, and efficiency, ICs are used in practically every electronic product today. Electronic devices would be more slower and larger without ICs. Furthermore, the widespread use of chips aided in the dissemination of advanced electronic gadgets to all corners of the globe.

(2)The Discrete Circuit is a circuit composed of individual electronic components connected together. If discrete components are used to implement circuits or systems with complex functions, it will inevitably result in a large number of components, increase in size, weight, and power consumption, and poor reliability.

(3) In comparison to discrete circuits, ICs have two major advantages: cost and performance. The cost is minimal because the chips are printed as a unit, with all of their components, rather than being built one transistor at a time, using photolithography. Packaged integrated circuits also utilize a lot less material than discrete circuits. Because of their compact size and close proximity, the IC's components flip quickly and require very little power. The fundamental downside of integrated circuits is the high expense of designing and fabricating the photomasks necessary. Because of the high initial cost, ICs are only financially viable when large volumes of production are expected.


Ⅳ. Why Integrated Circuit is shortage?

(1) Supply outnumbers demand.

With the rise of intelligent equipment in recent years, even the production of many items now requires clever equipment! As a result of the increased chip demand, a mobile phone now requires hundreds of chips to function, and an intelligent car will likewise require a large number of chips. As a result, demand is soaring, and several chip manufacturers are running out of stock!

(2) Issues with the manufacturing process

There is significant snow in a certain city in the United States at the time of the black swan in 2020, and that city happens to be where many silicon wafer producers converge. The chip fabrication speed has been slowed due to a power outage in Taiwan. There's also the drought in Taiwan, which is the worst in 50 years, making it difficult for TSMC and other chipmakers to secure enough water, which is necessary for chip manufacturing.

(3) The outbreak of the Covid-19 pandemic, which is the underlying cause of the catastrophe.

Consumers and organizations have begun to purchase new laptops and servers to satisfy the needs of professionals working remotely and youngsters learning at home as a result of the Covid-19 outbreak, which has resulted in a boom in demand for electronic items. As a result, despite a 6.5 percent drop in worldwide semiconductor sales between 2018 and 2019, sales in 2020 are expected to climb by 6.5 percent. In 2021, the fast expansion will continue. As a result, it's not surprise that manufacturers are having trouble keeping up.


Ⅴ. Where can I find Integrated Circuit?

Utmel Electronic is a reputable electronic component distributor. It has gained the trust of all clients due to its low price, quick delivery, and good quality. We stock a large variety of semiconductors, relays, boards, and modules, and we place a strong emphasis on customer service and technical assistance. You can get a free download of 10 million datasheets. To maintain regular production, 5 million alternative parts are required. To save time, we provide you with more rare components. More importantly, the data is updated and supplemented on a regular basis.


UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What role do integrated circuits play?

(1)Decrease the number of components used. Small-scale integrated circuits have reduced the number of content components and considerably improved discrete component technology since the invention of integrated circuits.
(2)The product's performance has been significantly improved. Integrating the components together not only lowers external electrical signal interference, but it also enhances the circuit design and speeds up the operation.
(3)More user-friendly application One circuit corresponds to one function, and one function is crammed into a single integrated circuit. In this approach, any function can be implemented to the relevant integrated circuit in future applications, considerably simplifying the process.

2.What is the function of an integrated circuit?

(1)The transistor is directly produced on monocrystalline silicon; (2) The components are densely integrated, and the wires are becoming increasingly thin, to the point where they are currently nanoscale thin; (3) The external connection lines are lead to the pins Place.

3.What's the difference between a microcomputer on a single chip and an integrated circuit?

(1) An integrated circuit is a circuit that connects several transistors, diodes, resistors (and sometimes capacitors) to build a circuit with a specific function and integrates them on a chip.
(2) An integrated circuit chip is a type of single chip microprocessor.
Related Articles

  • Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Saumitra Jagdale15 March 20242180

    For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.

    Read More
  • Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    UTMEL29 August 2025537

    This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.

    Read More
  • Xilinx FPGAs: From Getting Started to Advanced Application Development
    Xilinx FPGAs: From Getting Started to Advanced Application Development
    UTMEL09 September 202520

    This guide is your comprehensive roadmap to understanding and mastering the world of Xilinx FPGA technology. From selecting your first board to deploying advanced AI applications, we'll cover everything you need to know to unlock the potential of these remarkable devices. The global FPGA market is on a significant growth trajectory, expected to expand from USD 8.37 billion in 2025 to USD 17.53 billion by 2035. This surge is fueled by the relentless demand for high-performance, adaptable computing in everything from 5G networks and data centers to autonomous vehicles and the Internet of Things (IoT). This guide will walk you through the key concepts, tools, and products in the Xilinx ecosystem, ensuring you're well-equipped to be a part of this technological revolution.

    Read More
  • Advanced CMOS Devices with Wide Bandgap and Ultrawide Bandgap Technologies
    Advanced CMOS Devices with Wide Bandgap and Ultrawide Bandgap Technologies
    Saumitra Jagdale15 March 20242886

    Power and radio frequency electronics play an increasingly important role in energy-efficient and collaborative future as there is always a demand for faster, smaller, high-voltage and more conductive transistors. Traditionally, silicon has been the semiconductor of choice due to its extensive research and manufacturing history, and natural abundance. While silicon power devices continue to maximize performance, many applications are now integrating wider-band gap semiconductors. These materials offer a significantly higher voltage-conducting capacity, surpassing silicon's limits in tradeoffs related to ON-resistance, capacitances, and breakdown voltage.

    Read More
  • FPGA in Industry and Communication: Key Players, Technologies, and Future Trends
    FPGA in Industry and Communication: Key Players, Technologies, and Future Trends
    UTMEL07 March 20251052

    FPGAs (Field Programmable Gate Arrays) have become the core hardware in the industrial and communication fields due to their programmability and parallel processing capabilities.

    Read More